STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

where can i see backup file?

https://sips2017.sciencesconf.org/data/STM32CubeIntro_demo.pdf 50page show backup files.it explains that backup folder exists in Src folder in Project folder.but i check backup previous generated files when re-generating.but i can't find backup folde...

MYu.1 by Associate II
  • 933 Views
  • 0 replies
  • 0 kudos

Hi, I'm attempting to read memory data of my STM32F030c8t6_board (I got boards on banggood.com, picture in details section). I can not connect to my device. See details section for explanations. Best regards, Sylvain

Used tools:stm32cubeprogrammerSTLink-v2 (wired pins: 7:swdio, 9: swclk, 1: vcc, 8: gnd), the dev board usb is plugged to supply the chip.tried with all reset combinations, bus clock configs and boot0 config.tried with openocd as well (see console log...

0693W00000ANJFaQAP.png
sylvain2 by Associate
  • 3055 Views
  • 5 replies
  • 0 kudos

Resolved! where can i see information about STM32CubeProgrammer.

i use STM32CubeProgrammer.but i know that STM32CubePorgrammer don't support STM32G070RB(NUCLEO-G070RB).​STM32CubeProgrammer's Manual explains "STM32CubeProgrammer supports STM32 32-bit MCUs based on Arm®(a) Cortex®-M processors and STM32 32-bit MPUs ...

MYu.1 by Associate II
  • 2832 Views
  • 6 replies
  • 0 kudos

STM32CubeProgrammer error message !

I use STM32CubeProgrammer, but i can't use STME2CubeProgreammerI try to connect it to board, but error message happen.below error message.07:02:43 : ST-LINK SN : 066DFF383337554E4312365507:02:43 : ST-LINK FW : V2J37M2707:02:43 : Board    : NUCLEO-G07...

MYu.1 by Associate II
  • 1116 Views
  • 1 replies
  • 0 kudos

Resolved! Error: failed to download Segment[0]

HI, ST​Im trying to fw update using MFC Tool, STM32_Programmer_CLI.exe.​first, i checked that the fw download operation was completed using Terminal.so, I makeed the mfc tool in the way the terminal works in the background and checked the fw download...

JPark.20 by Associate II
  • 3448 Views
  • 2 replies
  • 0 kudos

STM32CubeProgrammer 2.7.0 released

New features• Added the support for the STM32WB15xx microcontrollers in the STM32WB Series• Added the support for the microcontrollers with 64 Kbytes of Flash memory in the STM32G0 Series• Added HardFault Analyzer support• Added Register viewer suppo...