STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer cannot connect to NUCLEO-F207ZG board in bootloader mode via UART interface

I have a NUCLEO-F207ZG board and STM32CubeProgrammer v2.7.0. I would like to use the embedded bootloader located in system memory. So, first I activate bootloader mode pulling-up pin 138 (boot0) of the MCU. Then, in order to verify this first operati...

RConf.1 by Associate II
  • 2192 Views
  • 1 replies
  • 0 kudos

Resolved! RAM parity function on the STM32G071RB breaks code execution? In short: When i clear the RAM_PARITY_CHECK bit in the option bytes (FLASH_OPTR bit 22), the program (in flash) will not run. Is this a hardware bug or am i doing something wrong?

I'm working on the NUCLEO-G071RB development board, using the IAR-EWARM (8.50.9) tool-chain.I've created a very basic program that only toggles user led (LD4) at 500ms intervals (using a wait loop with NOP instructions).The program doesn't use RAM (h...

EScho.2 by Associate
  • 2172 Views
  • 5 replies
  • 0 kudos