STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer v2.7.0-RC1 doesn't find target.

I am trying to debug small project on STM32H7B. I use STM32 Cube Programmer and STLINK-V3SET to clear the flash. It seems to me that ST-LINK GDB server ver 5.8.0 is connected. See blow.==========STMicroelectronics ST-LINK GDB server. Version 5.8.0...

NNari.1 by Associate II
  • 3029 Views
  • 4 replies
  • 0 kudos

Help connecting to STM32 on Cube Programmer

Hello everyone,I have a PCB with an embedded STM32F103 on it. The PCB provides access to some ports on the side. Those are linked to VDD, PA9, PA10, PA13, PA14 and GND. I tried connecting to it with Cube Programmer using a FT232RL as pictured below :...

0693W00000BZseOQAT.jpg 0693W00000BZsfRQAT.jpg 0693W00000BZsdqQAD.png
Math86 by Associate II
  • 5592 Views
  • 8 replies
  • 0 kudos

Resolved! CubeProgrammer UART Bootloader Error

Using STM32F412RGT6 on a board I've developed.having a problem using bootloader via UART (using CubeProgrammer).Following all described in AN2606.In my application, I'm using bootloader via UART1 (PA9, PA10).BOOT0 is High, BOOT1 is low while attempt ...

JUker by Associate II
  • 1538 Views
  • 2 replies
  • 0 kudos

External loader STM32L442 and S25FL127 Cypress

Hello all,I have written a External Loader using nucleo-l476rg and S25FL127 16mb NOR flash using 64k sectors. I was using it with TouchGFX and it worked just fine. I migrated to stm32l442. I have copied the code for the flash driver, changed the lin...

Future of STM32CubeProgrammer

Hi, I have a couple questions about the future of the programmer. 1) Are you planning to add self updating at any time? 2) This is really close to being a useful programmer on the production line. Basically it needs a way to save a configuration fo...

Resolved! Cann't open STM32_Programmer_CLI.exe

I have installed STM32CubeProgrammer 2.7.0 on Windows 10 and it works fine. but when iam trying to run STM32_Programmer_CLI.exe even as admin it open and close immediately. the same thing happens by openning the STM32Bootloader.batCould anyone tell m...

Dalhe.1 by Associate II
  • 14022 Views
  • 8 replies
  • 1 kudos

Resolved! ST-LINK_CLI.exe no full support for STM32G43x?

Hello, I was trying to set option bytes (BOR) with the ST-Link CLI (v3.6.0.0) for STM32G431, but it prompts that this feature is not available. With the ST-LINK Utility (v4.6.0.0) it is possible to set the BOR Level.I guess the ST-Link CLI is no long...

0693W00000AP9JCQA1.png
DKinz.1 by Associate
  • 1280 Views
  • 2 replies
  • 0 kudos