STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Getting "Device is under read out protection!" error when trying to program STM32F070RBT6 using USB port, Only on certain PCs

When trying to connect:When trying the same thing on a different PC (works on 3 different PCs, doesn't work on 3 other PCs). with the same IC it connects and programs with no issues.I checked the SW version of Cube programmer, on the 3 PCs that it wo...

0693W00000Kb1R2QAJ.png 0693W00000Kb1TnQAJ.png
AAlla.1 by Associate II
  • 3153 Views
  • 3 replies
  • 2 kudos

Resolved! STM32F411 Bricked after loading program

I have been programming with the STM32F411CE and I have now had this happen multiple times to different boards. Basically I program the board a few times and then all the sudden it will no longer connect. I get the following message from cubeIDE, STM...

KClos.1 by Associate II
  • 2741 Views
  • 4 replies
  • 0 kudos

Resolved! STM32CubeProgrammer v2.8.0 detects the wrong flash size for the STM32L152VDT6X causing the programming to fail

The STM32L152VT6X has 384KBytes of flash memory, but the STM32CubeProgrammer detects the flash size as being 128KB. When I try to flash an image of ~170KB it fails with the error "Operation exceeds memory limits". When I flash the same image with the...

0693W00000DnnbRQAR.png 0693W00000DnnbGQAR.png
AMT by Associate
  • 9662 Views
  • 14 replies
  • 3 kudos