STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! STM32CubeProgrammer v2.8.0 detects the wrong flash size for the STM32L152VDT6X causing the programming to fail

The STM32L152VT6X has 384KBytes of flash memory, but the STM32CubeProgrammer detects the flash size as being 128KB. When I try to flash an image of ~170KB it fails with the error "Operation exceeds memory limits". When I flash the same image with the...

0693W00000DnnbRQAR.png 0693W00000DnnbGQAR.png
AMT by Associate
  • 9989 Views
  • 14 replies
  • 3 kudos

Resolved! [H723] What file formats are supported by the firmware update? Can I find out more about the update?

H723ZGT6 Nucleo-144CubeMX 6.3.0CubePro​grammer [ data sheet ]   H723: DS13313 Rev2[Reference manual]   H723: RM0488 Rev2[User Manual] H723: UM2407 Rev 2​I'm currently investigating to implement the update feature.This time I will not use the bui...

0693W00000JOxHoQAL.png
june by Associate III
  • 3079 Views
  • 5 replies
  • 0 kudos

STM32CubeProgrammer_api project cannot run

hi,   I'm trying to run STM32CubeProgrammer_api project, I could build the STM32CubePrgAPI.exe with no error, but I got the 0xc000007B error when I run it; it seems that missing some runtime DLLs, I tried to install vs2015, vs2013, vs2010 runtime, bu...

szhih by Associate
  • 8765 Views
  • 17 replies
  • 0 kudos

STM32CubeProgrammer crashes when connecting to ST/Link

Hi: I've installed STM32CubeProgrammer and when connecting to the STLink debug programmer it worked ok. But now, it just crashes. I've tested three different probes, on two different computers.Both computers are running Linux (Arch Linux), kernel ver...

FDami.1 by Associate II
  • 1645 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.