STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

STM32G030K6T6 execute system memory bootloader, STM32CubeProgrammer connect ok, but can not program

Hi everyone, I use a JumpToBootloader( ) function in my code to execute system memory bootloader. and then STM32CubeProgrammer connect ok, but it can not program​MCU:STM32G030K6T6 STM32CubeProgrammer: v2.4.0Boot Interface: UART1 (PA9 PA10)+MAX13487EE...

0693W00000NsgxZQAR.png 0693W00000NsgxeQAB.png 0693W00000Nsgy3QAB.png

External Flash Loader on STM32G474 with SPI.

Hi,I'm trying to migrate an old firmware from a STM32F303 to a STM32G474.The MCU is related to an external Flash W25Q16JV.The old configuration uses the SPI bus to communicate with the external flash.So I changed the program in order to adapt the new...

MAmem.1 by Associate III
  • 1784 Views
  • 2 replies
  • 0 kudos

Resolved! Unable to connect to STM32H7 system bootloader via UART

I have been working with STM32H753 device. I was able to boot into the system booltoader of the Nucleo board. Cube Programmer was able to detect and connect through UART.But, I am unable to connect the Cube programmer in our custom board. Both BOOT_A...

SP.12 by Associate II
  • 3574 Views
  • 4 replies
  • 0 kudos