STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

I tried to program STM32F407 MCUs, using STLINK-V3MINI and STM32CubeProgrammer in automatic mode, but after first MCU, I'was not able to program any other MCUs. Someone could help me?

This is the log: 16:37:14 : STM32CubeProgrammer API v2.8.0 16:37:32 : ST-LINK SN : 003500125553500D20393256 16:37:32 : ST-LINK FW : V3J8M3 16:37:32 : Board    : STLINK-V3MINI 16:37:32 : Voltage   : 3.00V 16:37:32 : SWD freq  : 24000 KHz 16:37:32 : Co...

FCiuc.1 by Associate
  • 1102 Views
  • 1 replies
  • 0 kudos

Cannot Open file in STM32CubeProgrammer

Before this all work fine until suddenly the file cannot be open. Tried to uninstall and delete all related file form pc then install back. Tried also to download the new and old version. The result in the same for both, still cannot open file. Can s...

SBint.1 by Associate
  • 2138 Views
  • 4 replies
  • 0 kudos

STM32CubeProgrammer 2.10.0 released

STM32CubeProgrammer v2.10.0 release information New features • Added the updater tool for automatic software updates. The updater allows the users to make automatic updates of the software and its associated packages. It is available in all supported...

Cube Programmer can't find depencies

I just set up a new laptop and installed the Cube Programmer but I keep getting the error: CubeProgrammer_API or one of it's dependencies is missing. Please try reinstalling the program or check your java architecture.I am running Windows 10 64-bitI...

JKaz.1 by Associate III
  • 1518 Views
  • 1 replies
  • 0 kudos

CubeProgrammer connect to UART interface

I am using CubProgrammer (version 2.4.0) to update the flash on NUCLEO-G070 board.When I select the device target i/f as ST-Link and connect, I can do flash programming.When I select the target i/f is UART, the Com Port shows up correctly about this ...

KFang.1 by Associate II
  • 17715 Views
  • 10 replies
  • 2 kudos