User Activity

I have tested changing boot0 addresses for both the cores (M7 & M4) by STM32CubeProgrammer in ST-LINK mode. It is working properly.When I tried to implement same logic in SPI boot mode, M4_boot0 address is not updating. Where as M7_boot0 address is a...
Hi .I have STM32H745II controller, I am keeping its boot pin at HIGH state and providing reset condition.Host controller's SPI pins are connected to SPI3 pins PC10, PC11, PC12 and PA15 of STM32H745II for communicating in SPI boot mode.Here STM32H745I...
Hello Community.I am using STM controller STM32L432KC withBaud rate I have tried from 1200 to 115200.1 - stop bit9 bit data ( including parity ) as this is the only configure option available in STM32CubeIDE. Even Parity enable.1 - stop bit. as host ...
Hi .I am trying to program STM in boot mode. With controller operating on 3.3v with SPI speed less than 1.25MHz is working fine. While increase in SPI communication speed leads to get NAC not acknowledgment from STM controller in boot mode and i have...
Hello. I have STM3H723ZG Nucleo, by pulling boot pin high and providing reset condition, Nucleo stays in system bootloader mode. With Slave select low, I am send sync byte ( 0x5A) connections made over SPI3 port of STM32H7 controller form my Host con...
Kudos from