STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Resolved! External Memory Loader

Hello,I want to learn how to write my own octospi external memory loader in STM32CubeIDE. I found example on https://github.com/STMicroelectronics/stm32-external-loader/tree/main/STM32H7x_boards/MX25LM51245G_STM32H735G-DK but project is built with EW...

Louise by Associate II
  • 4233 Views
  • 2 replies
  • 0 kudos

Resolved! How do I re-program the STM32G0B1RET6 after I've done a "Full chip erase" in CubeProgrammer?

Hello i have a SKR board and the MCU was faulty. I swap the chip and tried to conect via SWD on CubeProgrammer but no success after i have can connect via usb but when i as to program by my mistake i erase full chip and after cannot conect again.Is t...

Resolved! Connection via SPI interface

According to UM2237, the Connect command in the CLI (command line interface) supports SPI, but what is the device used to connect the Nucleo board to the PC? How does the device look like from the PC side (device manager)?---> start (added to questio...

m.asada by Associate II
  • 5854 Views
  • 7 replies
  • 0 kudos

Resolved! Flash capacity of the STM32F723IC

Hello ST Community,I am currently working with the STM32F723ICT6. This has according to the datasheet (added as image) a flash capacity of 256 KBytes.While flashing with the STM32CubeProgrammer, which confirms the 256 KBytes flash capacity, I generat...

Rookie38 by Associate III
  • 2508 Views
  • 3 replies
  • 1 kudos

Resolved! "tm32cubeprog_v2-5-0": API-Error with Windows 7

Hello everybody,I am actually a PC software developer, but would like to be able to update the firmware of the hardware we have developed with our own software.For this purpose I have downloaded the "en.stm32cubeprog_v2-5-0.zip" and installed the Win...

Gneifel by Associate
  • 2805 Views
  • 3 replies
  • 1 kudos

Resolved! STM32H750 externalloader fails on SystemClock_Config.

Hi. I'm developing with custom board which has a custom QSPI (EN25QX128A - 16Mbytes flash), so I need to make an external loader used by STM32CubeProgrammer.First I wrote a code that interacts with QSPI and it works fine.So I changed this code to ful...

YNam.1 by Associate
  • 1298 Views
  • 1 replies
  • 0 kudos