cancel
Showing results for 
Search instead for 
Did you mean: 

I'm using the NUCELO-L152 and I want to sept the WRP bits with the cube programmer. When I set a bit and click on apply, I get the error message: "option Byte WRP does not exist". What is the process to set the WRP bits with the cube programmer?

JMene.1
Associate III
 
This discussion is locked. Please start a new topic to ask your question.
4 REPLIES 4
TDK
Super User

You might try the command line version instead. Perhaps it is named WRP1 and not WRP.

If you feel a post has answered your question, please click "Accept as Solution".
Houda GHABRI
ST Employee

Hi @JMene.1​ ,

I confirm there is an issue when configuring WRP option Byte for L152 family.

I will submit an internal ticket to CubeProgrammer development team but I need to be sure about this two points :

  • Are you using STM32CubeProgrammer 2.8.0 version?
  • Arre you using ST-Link connection?

Thanks for bringing this error to our attention.

Houda

JMene.1
Associate III

Thanks Houda. The answer is yes to both questions.

Houda GHABRI
ST Employee

Hi @JMene.1​ ,

Thanks for your feedback.

I submit an internal ticket to CubeProgrammer development team to debug further and fix the issue.

Houda