STM32CubeProgrammer (MCUs)

Ask questions on STM32CubeProgrammer and find answers on device detection, connection failure, programming issues, and more.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STM32CubeProgrammer v2.22 released

We are pleased to announce that STM32CubeProgrammer 2.22 is available What is new in 2.22: Support for the STM32U3 microcontrollers with 2 Mbytes of flash memory: Internal memory programming through debug and bootloader interfacesOption bytes program...

Problem to flash throught USB

Hello everyone,I have made a custom board with STM32L072CBT6. All works fine when i use my board and program her with STLink.I would try to program my board through USB, to do that i have a uUSB connector on my board connected to my uC. To flash, i u...

0693W00000Y7OsIQAV.png 0693W00000Y7Ox7QAF.png
MLam by Associate III
  • 1881 Views
  • 1 replies
  • 0 kudos

Resolved! STM32F7 dual bank mode vs flashing tools

Don't have a eval board currently, waiting for order to arrive.Can anyone tell whether CubeProgrammer and other popular tools will properly detect that F7 is in dual bank mode, so it has a different number and size of sectors?Can these tools set the ...

Pavel A. by Super User
  • 2030 Views
  • 2 replies
  • 0 kudos

Hi all, MCU we are using is :- STM32G0B1CE During factory manufacturing we have notice some issues where MCU does not enumerate the comport.

We have seen several signatures of this issue.Signature 1:The extracted binary shows that the image is located on Bank1. Also the extracted byte options show that the image should be located on Bank2 but it was empty and still the device boots up aft...

Kpodu.1 by Associate II
  • 2122 Views
  • 3 replies
  • 0 kudos

Resolved! STM32CubeProgrammer (cli) chunk size setable?

Heyin a project of us we are using the legacy STMFlashLoader to flash firmware on a STM32F103 via the system bootloader on UART1, but wanted to migrate to STM32CubeProgrammer now. In this application the PC (Win10) which runs STMFlashLoader/STM32Cube...

waldmanns by Associate II
  • 1738 Views
  • 1 replies
  • 1 kudos

Resolved! STM32CubeProgrammer USB DFU not detected on linux

Hi,USB DFU did not work in STM32CubeProgrammer in Linux. The programm did not detect the usb port. But it works faultless in STM32CubeProgrammer in windows.I tested with STM32CubeProgrammer V2.10 and 2.12, same results.I have linux mint 20.3 Luna

0693W00000WL7ZIQA1.png
VNong by Associate II
  • 11934 Views
  • 4 replies
  • 1 kudos