2021-11-30 3:17 AM
Hey,
today I update CubeIde to 1.8 (with new CubeProgrammer 2.9) and noticed that I can no longer flash my external QUADSPI memory as I used to before in version 1.7. I made custom external loader following this guide : https://www.st.com/content/st_com/en/support/learning/stm32-education/stm32-moocs/external_QSPI_loader.html
Is there anything I need to change in my loader ? Or there is new bug present ?
I get this console output:
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
LogFile Name : D:\Work\STM32CubeIDE\Projects\OB_TP-H7\V1_0\OB_TP-H7\Debug\st-link_gdbserver_log.txt
Logging Level : 31
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Enabled
SWD Debug : Enabled
InitWhile : Enabled
COM frequency = 24000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fefd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V3J9M3B5S1
Device ID: 0x450
PC: 0x8004d40
ST-LINK device status: HALT_MODE
ST-LINK detects target voltage = 3.29 V
ST-LINK device status: HALT_MODE
ST-LINK device initialization OK
Stm32Device, pollAndNotify running...
SwvSrv state change: 0 -> 1
Waiting for connection on port 61235...
Waiting for debugger connection...
Waiting for connection on port 61234...
Accepted connection on port 61234...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61234...
GDB session thread running
GdbSessionManager, session started: 1
Accepted connection on port 61234...
Debugger connected
Waiting for debugger connection...
Waiting for connection on port 61234...
GDB session thread running
GdbSessionManager, session started: 2
Stm32Device, closeDevice() entry
GDB session, device event: 5
GDB session, device event: 5
Stm32Device, pollAndNotify stopped
Stm32Device, closeDevice() exit
------ Switching to STM32CubeProgrammer -----
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : 002400235553500F20393256
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3.29V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x450
Revision ID : Rev V
Device name : STM32H7xx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M7
BL Version : 0x90
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_a15960.srec
File : ST-LINK_GDB_server_a15960.srec
Size : 2331676 Bytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 8]
Erasing memory corresponding to segment 1:
Erasing external memory sectors [0 307]
Download in Progress:
�������������������������������������������������� 0%
����������� 22%����������� 44%����������� 66%
Error: failed to download Segment[1]
Error: failed to download the File
------ Switching context -----
COM frequency = 24000 kHz
Target connection mode: Under reset
Reading ROM table for AP 0 @0xe00fefd0
Hardware watchpoint supported by the target
ST-LINK Firmware version : V3J9M3B5S1
Device ID: 0x450
PC: 0x8004d40
ST-LINK detects target voltage = 3.30 V
ST-LINK device status: HALT_MODE
GDB session, device event: 6
GDB session, device event: 6
Stm32Device, pollAndNotify running...
GDB session, device event: 3
GDB session, device event: 3
GDB session, device event: 1
GDB session, device event: 1
GDB session terminated: Client connection lost
GdbSessionManager, session terminated: 2
Cleanup session: 2
GDB session disposed: 2
Received Ctrl-C from the client
ST-LINK device status: RUN_MODE
Device not halted(0), performing Ctrl-C
GDB session, device event: 4
Device halted
GDB session terminated: Client connection lost
GdbSessionManager, session terminated: 1
GdbSrv, master session terminated, signal dispose
Shutting down...
Stopping port 61234
Received stop for port 61234, not accepting new connections.
GdbSrv, deInit entry.
GdbSessionManager, deInit entry.
ST-LINK device status: HALT_MODE
GDB session disposed: 1
GdbSessionManager, deInit exit
SwvSrv deInit entry
Stopping port 61235
Stopping port 61234St link log file is also attached.
2021-11-30 4:08 AM
Let us try to conclude whether the problem exist in CubeProg stand-alone also or if there is an issue in the interface between CubeIDE / CubeProg.
Reading your log-file we can see that CubeProg is invoked using the following command line arguments:
C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\STM32_Programmer_CLI.exe --connect port=SWD speed=fast sn=002400235553500F20393256 mode=UR reset=hwRst --extload C:\ST\STM32CubeIDE_1.8.0\STM32CubeIDE\plugins\com.st.stm32cube.ide.mcu.externaltools.cubeprogrammer.win32_2.0.100.202110141430\tools\bin\ExternalLoader\MX25L12833FM2I_TP-H7_STM32H753IIT6.stldr --download c:\path\to\project.elf –verifyc:\path\to\project.elf to be substituted with your path in the project...
Does that work? If so, then we have to analyze in the IDE-team.
If not, then the issue is probably in CubeProg it self...
If it did not work, could you also please try the CubeProg GUI version to perform the same operation?
You could also try to perform a mass erase on the flash, sometimes that helps...
Let us know your findings.
2021-11-30 5:09 AM
Hey @mattias norlander , I tried to run this command and got the same result.
In GUI version of STM32CubeProg 2.9 I also can't flash my program to board. Mass erase is also not helping. Check CubeProg GUI version log file in attachment.
But I noticed I can normally mass erase/sector erase/read and write data to external flash.
So there must be a problem with new STM32CubeProgrammer.
2021-11-30 6:50 AM
Thanks for the tests!
Here are my train of thoughts:
That said, I don't want to jump to any conclusion.
I will pass this thread internally to someone in CubeProg team for further analysis.
@Nawres GHARBI, could you have a look?
Kind regards, Mattias
2021-11-30 7:50 AM
@mattias norlander thank you for your time and fast replies. I hope they can reproduce this issue and find where the problem is.
2021-11-30 10:50 PM
For the purpose of tracking I provide our internal ticket reference: 118715.
2021-12-06 11:10 PM
Hello,
Similar problem with internal flash?
I work with a STM32L4R9 project and TouchGFX. This device is 2MByte flash size, but debug parse elf file with only one MByte of à 1.9mByte binary code.
That works with CubeIde 1.7 but fails with new 1.8 and CubeProgrammer 2.9, only BANK1 is flashed.
STMicroelectronics ST-LINK GDB server. Version 6.0.0
Copyright (c) 2021, STMicroelectronics. All rights reserved.
Starting server with the following options:
Persistent Mode : Disabled
Logging Level : 1
Listen Port Number : 61234
Status Refresh Delay : 15s
Verbose Mode : Disabled
SWD Debug : Enabled
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
Debugger connected
Waiting for debugger connection...
-------------------------------------------------------------------
STM32CubeProgrammer v2.9.0-RC01
-------------------------------------------------------------------
ST-LINK SN : XXXXXXXXXXXXXXXXXXXXXXXXXXX
ST-LINK FW : V3J9M3B5S1
Board : STLINK-V3SET
Voltage : 3,30V
SWD freq : 24000 KHz
Connect mode: Under Reset
Reset mode : Hardware reset
Device ID : 0x470
Revision ID : Rev W
Device name : STM32L4Rxxx/STM32L4Sxxx
Flash size : 2 MBytes
Device type : MCU
Device CPU : Cortex-M4
BL Version : --
Debug in Low Power mode enabled
Memory Programming ...
Opening and parsing file: ST-LINK_GDB_server_RxvN6O.srec
File : ST-LINK_GDB_server_RxvN6O.srec
Size : 1 MBytes
Address : 0x08000000
Erasing memory corresponding to segment 0:
Erasing internal memory sectors [0 255]
Download in Progress:
Error: failed to download Segment[0]
Error: failed to download the File
With CubeIde 1.7 sectors [0 417] are used
----------------------------------------------
And when flashing binary generated by CubeIde 1.7 with new STM32CubeProgrammer interface 2.9 :
08:02:18 : Memory Programming ...
08:02:18 : Opening and parsing file: XXXXXX.bin
08:02:18 : File : XXXXXX.bin
08:02:18 : Size : 1710704 Bytes
08:02:18 : Address : 0x08000000
08:02:18 : Erasing memory corresponding to segment 0:
08:02:18 : Erasing internal memory sectors [0 417]
08:02:27 : Download in Progress:
08:02:27 : Error: file size is bigger than the flash memory size.
08:02:27 : Error: failed to download Segment[0]
08:02:27 : Error: failed to download the File
Regards
2021-12-07 6:08 AM
@Community member so I'm not the only one with this problem.
@mattias norlander and @Nawres GHARBI any news about that ?
2021-12-07 7:39 AM
Dear all,
I reported a similar problem on the Discovery STM32L5 board (https://community.st.com/s/question/0D53W00001EywtESAR) For me it is very likely due to the STMicroelectronics ST-LINK GDB server. Version 6.0.0. In CubeIDE 1.7 this was version Version 5.9.1. The standalone STM32CubeProgrammer (2.8 and 2.9) work in my case. So its more likely the combination STM32CubeIDE + ST-LINK GDB.
I actually disagree to consider this thread as 'answered' like it is shown in the overview.
Best Regards
Markus
2021-12-30 5:39 AM
Do you have any minimal example projects where you can reliably re-produce the issue?
That would help the troubleshooting!