STM32 MPUs Embedded software and solutions

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32 board support eDP bridge?

Hi,We are using stm32mp157c MCU/board and it has DSI output built-in. Now we want to add display port support via DSI to eDP bridge SN65DSI86. It seems that stm32 does not support Displayport output or it has never been done. At least the driver dw_m...

LLe.1 by Associate II
  • 4691 Views
  • 34 replies
  • 0 kudos

Ethernet not working when PHY configured in MII mode in custom board using a STM32MP153CA + automotive Ethernet PHY NXP TJA1101.

I cannot make the Ethernet work on my custom board (STM32MP153CA + automotive Ethernet PHY NXP TJA1101) in U-BOOT (haven't even tried loading kernel). The PHY is connected to an external 25MHz xtal. I'm working with 5-10-dunfell-mp1-21-11-17 files in...

LCast.2 by Associate II
  • 2336 Views
  • 5 replies
  • 0 kudos

Resolved! USB compliance testing

Hi, and yet another question...We would like to perform electrical compliance testing on our USB ports. This requires each port to send a test pattern.Our board has one upstream and two downstream facing ports. The upstream port can be set into vario...

jvog.sen by Associate II
  • 1350 Views
  • 2 replies
  • 0 kudos

Stm32mp157a dac dma issue

Hi,We are using Stm32mp157a processor in my custom board.We are trying to work on dac with DMA but it is not working.You can see my configurations below.In cube mx for DAC there is no Dma option.so we added DMA manually with reference Stm32mp1 Uart ...

DMA2 RX stream5 CM4 not working

Hello , I am trying to configure RX (only) with dma. I am using DMA2 stream5 on usart3 I have connected USB to UART bridge (4 wire) on 40 pin headers RX,TX,VDD(3) and GND on CN7. Whenever I am trying to send any data from the comport (teraterm ) fro...

PVaaz.1 by Associate III
  • 512 Views
  • 2 replies
  • 0 kudos