STM32 MPUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Firmware Deployment on STM32MP157D M4 Core

I am working on building a Yocto-based Linux distribution for the STM32MP157D SoC. I have already set up the process to build the Linux image successfully. However, I need guidance on the following:Deploying Firmware on M4 CoreWhat is the correct pro...

Mohand by Associate
  • 295 Views
  • 1 replies
  • 0 kudos

Resolved! Error activating spi module in Yocto Linux project

Hello,I have a Yocto Project with st-stm32mp1 layer, using Poky distribution along with customized CubeMX machine that I created using st-stm32mp1-addons layersI need to use the spi5 module, so I activated it through CubeMX for the "A7NS" runtime con...

thp9 by Associate II
  • 1625 Views
  • 6 replies
  • 0 kudos