STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

ADC usage with MP135-DK in Linux

I having some difficulties figuring out details about the ADC usage under Linux, in particular on the MP135F-DK.I located the io driver sources, and the drive itself seems to work:Checking the board user manual, the GPIO pins PC2 and PC3 are routed o...

Ozone_0-1731148007807.png
Ozone by Principal III
  • 1070 Views
  • 1 replies
  • 0 kudos

PHYTEC STM32MP135 LCD PANEL DTS

Hello everyone,I am using the STM32MP135 SoM from PHYTEC, and I’m creating a custom device tree source (DTS) file tailored to our carrier board. I’m having trouble controlling the backlight PWM signal. I’m unable to enable the PWM and enable signal a...

image_2024-11-05_005132081.png image_2024-11-05_005307530.png image_2024-11-05_005326551.png
batuhanky by Associate III
  • 2197 Views
  • 3 replies
  • 1 kudos

STM32MP135 NO BACKLIGHT

Hi Everyone,I have problem with custom carrier and dts. I am using MP135 SoM from PHYTEC and when I add panel backlight property to the panel node, there is no pwm output, but when I comment out this feature from the panel node, the panel backlight w...

batuhanky by Associate III
  • 1265 Views
  • 0 replies
  • 0 kudos

PWM backlight not working.

Can you please check my device tree configuration?Backlight as a GPIO is working correctly, but when i try to use it as pwm, the pin line is always fixed to low.Inside my .dts:This is my panel definition:panel { compatible = "newkoro,display","simp...

Lmoio.1 by Senior
  • 9235 Views
  • 10 replies
  • 0 kudos