Can I Use rts-gpios in the Device Tree or is it not supported
stm32mp157f, I need to use uart5 to drive an rs485 but the hardware supplied DE pin is already in use. So I need to configure a different GPIO to use. If the device tree binding rts-gpios is supported, then the task is simplified. We can modify the...