STM32 MPUs Embedded software and solutions

Ask questions and find answers on STM32 microprocessors and dedicated embedded software solutions, such as Yocto SDK, Qt, and OP-TEE.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

configure stm32MP1 I2S

Hello sir I am using stm32MP157 with ICS-43434 sensor via the I2S interface   I am following "https://wiki.st.com/stm32mpu/wiki/I2S_Linux_driver" link to enable the I2S driver in my "make menuconfig" the "STM32 I2S interface (SPI/I2S block) support" ...

pragnesh by Associate III
  • 1572 Views
  • 1 replies
  • 0 kudos

Not able to see the SPI in /dev.

we are using stm32mp157f-ev1 and we build the weston image for this board.We want to enable the SPI-1 on this boardwe had applied the following patch to enable the SPI-1+&spi1 {  +       status = "okay";  +       pinctrl-names = "default", "sleep";  ...

HVerm.3 by Associate
  • 2757 Views
  • 2 replies
  • 0 kudos

Max clock for I2C for stm32mp157a

I have several questions first one is what is the max clock for I2C, minimum is pointed at this sheet but what is the max?Again for the same sheet for the LCD-TFT controller, I will be using 1.8V LVDS display so fclk frequency will be 45 MHz max righ...

Gencay by Associate III
  • 1999 Views
  • 1 replies
  • 0 kudos

Resolved! QSPIO NOR flash connected to STM32MP153CA bank1 does not work in U-Boot. sf probe 0 fails to initialize spi flash with error -22

I cannot get the QSPI NOR-Flash to work on my custom board using an STM32MP153CA + Adesto AT25SF128 NOR flash in U-BOOT. I'm working with 5-10-dunfell-mp1-21-11-17 files included on the 3.1.0 ecosystem.The schematic section is shown below:Is not tha...

0693W00000QMZ9BQAX.png
LCast.2 by Associate II
  • 2434 Views
  • 1 replies
  • 0 kudos