Getting started with STM32MP1
Hi,I’m new bee to to this processor based development.I’m currently starting with STM32MP1 can someone help me what tools are required to start exploring
Hi,I’m new bee to to this processor based development.I’m currently starting with STM32MP1 can someone help me what tools are required to start exploring
Which OS can be best compatible for STM32MP135F-DK processor? Is it feasible to use ubuntu or debian where I can use yocto build?
Dear ST community,I am currently trying to install an 8bit 8080 LCD , and i figured out that it needs FMC $ to be set up in devicetree in order to interface with it using DRM in Linux. i have the following device tree pinctrl nodes setup fmc_pins_m...
Hello,I'm trying to configure an externall interrupt (for a digital signal) to be handle from the User Space. I have configured the following node in the device tree on the root node:/ {... exti_gpio_node { compatible = "test,button"; ...
1、Part Number:STM32MP135FAE7 2、tzc_it_handler:72 TZC permission failure3、Environment:PC:ubuntu18,environment-setup-cortexa7t2hf-neon-vfpv4-ostl-linux-gnueabi,arm-ostl-linux-gnueabi4、We designed a STM32MP135 based SOM, using the ST I2C PMIC, STPMIC1D,...
Hello everyone,I am working on a custom board based on stm32mp15x. I am trying to periodically wake up my system from the shutdown condition using the RTC. From the hardware point of view, I am using the STPMIC to restore the Vdd supply of the MPU, w...