Load Bin Using RPROC
Hello Iam Using Stm32mp157aaa3 processor in my custom board and U boot version 2023.10.Can we load .bin extension file using rproc command in uboot. Tanks & RegardsSrikanth.R
Hello Iam Using Stm32mp157aaa3 processor in my custom board and U boot version 2023.10.Can we load .bin extension file using rproc command in uboot. Tanks & RegardsSrikanth.R
I wrote u-boot video driver for my board. Everything is fine but I cant find the place where STMLinux disables the DSI power loading the kernel. Has anyone succeeded in keeping the u-boot splash screen on during the boot?
Im attempting to set up A/B partitioning on an STM32MP157d-dk1 board so that it can switch between partitions when updating. The board image is built using yocto, and I have used the meta-st-stm32mp layer, and am building a modified version of core-i...
Hi there, During OP-TEE integration of our custom platform based on STM32MP151C MPU I'm facing an issue with DFU. It looks like the dfu command stucks in `run_usb_dnl_gadget` inside the loop and waits forever for the flush flag: NOTICE: CPU: STM32MP1...
When I start uboot it says MMC: STM32 MMC: SD/MMC:0 and STM32 SD MMC: 1 but then it won't boot linux saying "No block device". I have looked at the eval board DTS and tried to include as much relevant items as I could but am not getting any signs of...
Hi there,I currently work on the integration of OPTEE to our custom STM32MP151C-based platform. The problem that I've faced is that U-boot hangs just after the board_init_f() function and relocation procedure: NOTICE: CPU: STM32MP151CAC Rev.ZNOTICE:...
Hello, I want to boot Linux straight from the FSBL, avoiding SP-Min and U-Boot. Is there any configuration or information on how to do this? Thank you. I got a STM32MP157F-EV1 board, I wouldn't mind using TF-A or U_Boot SPL, I am also looking at ...
HI,I am working on a custom STM32MP151AAC3 board, and working on OpenSTLinux 4.10 distribution package.Now I can connect to the board through UART4(PB2 and PG11) by STM32CubeProgrammer, and I want to tune the DDR3 to verify the design. I need the u-b...
Hello everyone,I have the stm32mp157c-dk2 for performance evaluations. Our goal is to check if the CPU/GPU performance is good enough for our next productm which will be used as a GUI frontend.I built the openstlinux (mickledore) as-is from github su...
I'm having trouble in bringing up my custom board. I've made a custom device tree using CubeMX and adding the sections as described in "Lab-MP15_FromPartNumber_To_BasicDeviceTree_with_CubeMx". I can program fsbl-boot and fip-boot, but i'm not able to...