Resolved! LPTIM_TypeDef contains incorrectly sized field uint16_t RESERVED1
The LPTIM_TypeDef struct that is used throughout many of the HAL header files contains a few RESERVED fields that cover unused address offsets in the peripheral's memory map.The first of these, RESERVED1, is declared as uint16_t. I believe that this ...