STM32 MPUs Embedded software

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Problems with DCMI DMA callback registration. Environment: MCU: STM32MP157/M4; SW: STM32Cube FW_MP1 V1.6.0; Engineering Boot Mode

Hi all!Environment: I use MX to configure the DCMI Peripheral including DMA!MX generates MX_DMA_Init() and MX_DCMI_Init()After DCMI initialization in main with the above mentioned functions I use the functions HAL_DMA_RegisterCallback(&hdma_dcmi, HAL...

MLENG.1 by Associate
  • 597 Views
  • 1 replies
  • 1 kudos

Can't Burn eMMC with DCMI camera plugged

Hi, i moved to new ecosystem v2.0 "dunfell" and added my layers of wifi,camera, openCV and python packages from old Yocto ecosystem. when i trying to burn my custom board eMMC with my dcmi camera plugged it stuck on U-boot waiting for the USB connect...

SMich.1 by Senior
  • 453 Views
  • 8 replies
  • 0 kudos