User Activity

Hi,I am trying to migrate my project (custom board using stm32mp153a and 256MB mem) from 4.1.0 to 5.0.0 but I am getting a panic when booting u-boot:Board: MBfdd8 Var2.15 Rev.B-14 DRAM: 256 MiB E/TC:0 tzc_it_handler:79 TZC permission failure E/TC:...
I am trying to migrate from ecosystem 4.1.0 to 5.0.0 however after getting all the device trees to compile and build plus a new image I am encountering a Panic in optee. The problem is that it just says Panic and I can't tell based on the debug print...
Is there a walk-through or example of how to setup secure boot using a custom device tree?As a side note, the following page returns "Permission Error", is that expected behaviour?https://wiki.st.com/stm32mpu/wiki/STM32MP15_secure_boot
I am trying to configure a DMA stream to capture the RX channel of a UART core on the m4, however, I get very undesirable behaviour.I am trying to set up a circular rx buffer that is of size 10 since the data coming back is of multiples of 5. Unfortu...
Is HAL_UARTEx_ReceiveToIdle_DMA supported on STM32MP15 products? If so is there an example for using it?
Kudos from