BOOT PROCESS - STM32MP157A-DK1
HI STM32 Team,What is the boot process of STM32MP157A-DK1 BOARD and where to study that. Thanks in advance,Regards,A. Ajith Kumar
HI STM32 Team,What is the boot process of STM32MP157A-DK1 BOARD and where to study that. Thanks in advance,Regards,A. Ajith Kumar
I have to deploy a NN on this device and I want to optimize cache for improving the energy efficiency.
Hi, I'm reading up on stm mp1, in particular the Linux side, my intent was to use the M4 to read data from sensors and transfer them to the A7 on the Linux side. Now I've read the function in C code that reads the messages from the manual: read:int r...
Hello, i am working on the STM32MP157C to use its ADCs. at first i was only using the iio framwork on linux , however it is limited. so i'm trying the examples on the (github page) using the Linux Remoteproc . my board configuration is different sinc...
Hello,I am facing the issue below when build up my image (or u-boot-stm32mp alone)I mainly followed instructions in https://wiki.st.com/stm32mpu/wiki/How_to_compile_the_device_tree_with_the_Distribution_Package.But it did not work.make -f /home/luisa...
HelloI hope you are doing wellI read the TF-A documentation and I found out that there is a POC for TPM service that measures event logs during startup. Source: https://trustedfirmware-a.readthedocs.io/en/latest/design_documents/measured_boot_poc.htm...
i am using openstlinux starter package use in stm32mp135-dk. i want to know how to upload a video in sd card of board and also how to play in board.
Hi,I am new in STM32MP1 MPU Linux and wish to get the guiding to start developing Linux OS app for my board. The first question:I need to switch GPIO pins. Any suggestions where to start for single core MPU STM32MP135. Thanks.
Dear All, I have followed the instruction as per Intro to Embedded Linux Part 2 - Yocto Project.The compilation for layer kirkstone. When i run the command "bitbake core-image-minimal" it give error after 4 hours of work.The error is pasted below./ho...
Hello,we have developed a project in STM32CubeIDE which already works.the the project is generated "Under Root" like this: Now we want to implement the compilation in a yocto layer instead of use .elf directly.we have take into account the extended...