STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STSAFE

Hi,How to authenticate a  device connected to STM 32 using USB Peripheral the STM 32 is integrated with STSAFE  IC , How to use peripheral Authentication Example for this in the software package 

SBSFU integration with STM32 L496ZG

I am integrating SBSFU with the STM32L496ZG microcontroller and have created a new project. I attempted to generate the SFB file using a customized post-build script from the L476 Simple App example. Although I modified the script paths for my projec...

STSAFE-A110 and hardware-level security

I'd like to open a small discussion about what would be the best usage of STSAFE-A110 to enhance the hardware-level security of our IoT device. To be more specific, in our application we want to use the STSAFE-A110 to store the customized device priv...

naNEQ by Associate II
  • 1926 Views
  • 1 replies
  • 0 kudos

Enable TrustZone without using STM32Programmer

Hello,I am working STM32u575 Nucleo board. I want to use secure flash to store secure data and to use it I need to enable TrusZone. Is there a way we can program option bytes with TZEN =1 without using STM32programmer?Regards,Shafi

Shaffi by Associate II
  • 1579 Views
  • 2 replies
  • 0 kudos

Resolved! STM32U585:FLASH Read protection level 1 issue

Dear Sir/Madam We are using STM32U585AII6Q MCU part in one of our projects. We encountered a problem with Flash read protection and no longer able to flash the MCU. Below is the reference screenshot from the error. We also tried few methods defined ...

apoorvabs_0-1728648184182.png
apoorvabs by Associate II
  • 2962 Views
  • 4 replies
  • 2 kudos

Resolved! Need help on writing into secure flash in STM32U575

I am working on STM32U575 to write and read from Secure flash. I referred   STM32Cube_FW_U5_V1.4.0\Projects\NUCLEO-U575ZI-Q\Examples\FLASH\FLASH_EraseProgram_TrustZone\but I was facing following issueCan you please help me resolving it. Do we have an...

Shaffi_0-1728377891530.png
Shaffi by Associate II
  • 3612 Views
  • 7 replies
  • 0 kudos

RCC_CSR registers with SBSFU

Hello,I am working with SBSFU on a STM32U575 microcontroller and have written a function to check the cause of the system reset by reading the flags from the RCC registers using __HAL_RCC_GET_FLAG. However, the issue is that none of the RCC register ...

Resolved! SFI without TrustZone on STM32U5 is possible?

I need to perform SFI on an STM32U599 MCU, so following the wiki article "SFI Step-by-step on STM32 boards" I prepared the firmware and programmed the HSM V2 smartcard.I'm sending the commandSTM32_Programmer_CLI -vb 1 -c port=SWD mode=HOTPLUG -sfi xx...

paolog by Senior
  • 3993 Views
  • 7 replies
  • 0 kudos

SBSFU with wolfssl in stm32h7

Hi,I am trying to replace mbedTLS library with Wolfcrypt library for crypto operations in SECoreBin project of SBSFU. I was able to replace SHA256 related APIs. But the bootloader is crashing when I try to initialize wolfssl ECC key object under SE_C...

h_adi by Associate
  • 1053 Views
  • 1 replies
  • 0 kudos