STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

About OEMiROT_Appli_TrustZone for H563ZIT6 SBSFU

Hi, I use OEMiROT_Appli_TrustZone +OEMiROT_Boot to do some change in order to migrate to my project. Version: STM32Cube_FW_H5_V1.5.0 1.i change the secure image and non secure image size in flash_layout.h from OEMiROT_Boot. #define FLASH_S_PARTITION_...

hongjin by Associate
  • 147 Views
  • 1 replies
  • 0 kudos

STM32U5 HASH

Post edited by a ST moderator to be inline with the community rules especially on the code sharing. In next time please use </> button to paste your code. Hi I am struggling getting context save restore working correctly, when operating the HASH hard...

aes2 by Associate II
  • 228 Views
  • 1 replies
  • 0 kudos

Download .sfi file to stm32h753 use HSM

I got an error when downloading the .sfi file to STM32H753II using the STM32Programmer_CLI, my HSM version is V2AE.The error message is as follows:What its mean?V2AE cannot support STM32H753,and must use HSM_V1?or H753 cannot support SFI ?I’m a new u...

SONGTAOSI_0-1776668414194.jpeg

Loading New Firmware onto Write-Protected STM32 B-U585I

Hello, I am working with an STM32 B-U585I development kit. The board has been previously used, and some protection-related configurations have been modified. I am now trying to perform new tests on the device, but I believe I am unable to bypass the ...

Fega by Associate
  • 144 Views
  • 1 replies
  • 0 kudos

Wild issue! STM32H7S78 stuck after DA provisioning!

OverviewDebug Authentication Discovery occasionally succeeds in CLOSED state, but Full Regression fails (“Unable to boot on RSS_DA” / “Unable to detect DBGMCU Mailbox”)Get ready for the stm32 safari! Product / Environment- Board: Custom based off of ...

R_1 by Associate III
  • 447 Views
  • 5 replies
  • 0 kudos

SBSFU - Build Structure

Hi everyone,I’m currently working with STM32 Secure Boot and Secure Firmware Update (SBSFU) and integrating it with my custom application. I’m trying to design the project in a modular and scalable way for long-term use, and I would really appreciate...

H573 Trust Zone / Secure Boot support in Zephyr MCUBoot

HiI've been trying to understand what level of support is available for the H573 security features in Zephyr RTOS with mcuboot but either can't find any information or no one replies to my comments.I have a Zephyr sysbuild build working where mcuboot...

ekwus by Associate II
  • 1642 Views
  • 4 replies
  • 0 kudos