STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STM32H563VG chip cannot be erased

Hi,I'm using an STM32H563VG (1MB Flash version) on a custom board. I have a STLINK-V3MINIE connected and I'm using STM32CubeProgrammer.When I'm doing a full chip erase, the content of the flash memory is not altered, everything is still there when I ...

CClau.1 by Associate II
  • 1096 Views
  • 2 replies
  • 0 kudos

SFI programm STM32L562 do not work.

Good day!I have custom board with cpu stm32l562. I am prepared all data and global license. CPU prepared by script file from package STM32CubeExpansion_SFI_v1.5.0 L5.This operation is OK.But after if start programm by Cube Programmer ( v 2.19 ) - i h...

dlpPavlo by Associate II
  • 1270 Views
  • 5 replies
  • 0 kudos

STM32H730 AES-GCM Tag issue

STM32H730, an invalid tag is generated for payloads that are not a multiple of 4, as described in Re: STM32U545 AES GCM Tag mismatch - STMicroelectronics Community.AES-CCM: no issues, everything works.AES-GCM:The HAL already handles required padding ...

GCern.1 by Associate III
  • 4605 Views
  • 9 replies
  • 1 kudos

Information about MCUboot and illustrative examples

Hello everyone, I'm learning about MCUboot. Currently I have tried searching for information online but still don't have an overview. So I hope everyone shares their experiences about MCUboot (things to learn here) and give me some programs to better...

OEMUROT Boot jumping address clarification

Hello, I have been modifying the OEMUROT_Boot application and associated build scripts in ROT provisioning to complement our custom firmware project. (See my previous post on this topic for details). This is for the STM32N6, using the DK discovery ki...

hnHSD by Associate II
  • 1050 Views
  • 4 replies
  • 0 kudos

Resolved! STiRoT Boot Time

Hello,I'm a developper from the CEA using STM32H573 and I am characterizing the chip boot time in various configurations. With STiRot activated (250 MHz and a 128 Kb image) I found 31 ms which is twice as much as the boot time indicated in the docume...

halwizard by Associate II
  • 1616 Views
  • 5 replies
  • 0 kudos