STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Should SFU_LL_Flash_Write be aligned to 64 or 32 bit?

In the code it says the following:/** * @brief This function writes a data buffer in flash (data are 32-bit aligned). * @note After writing data buffer, the flash content is checked. * @param pFlashStatus: FLASH_StatusTypeDef * @param pD...

Arno1 by Senior
  • 1203 Views
  • 1 replies
  • 0 kudos

Resolved! Require authentication for firmware update

I started a new project, and my security requirement states that user authentication is required when updating firmware.I wonder if there's a feature for this, and if not, can the bootload side be modified to meet this requirement?I searched and foun...

DPark.2 by Associate II
  • 2442 Views
  • 4 replies
  • 0 kudos

How can I get Atollic to append a CRC to the flash image?

IAR would fill unused flash and optionally append a crc to aid with the integrity check some of us need to do for regulatory compliance But since IAR's been replaced what provisions are in Atollic to fill unused flash and optionally append a crc? Is ...

n2wx by Senior
  • 2778 Views
  • 6 replies
  • 0 kudos

Please Let me know correction in below code or this code is correct or not . I am doing first time in AES256 Security . any help is highly appreciated .

I wants to encrypt 8bits of data using AES256 Security with STM32L442KC . And sending Encrypted data through UART. I am confused in code that code is correct or not....please let me know any correction in this code. I am using Atolic true studio.u...

STAR by Associate II
  • 902 Views
  • 0 replies
  • 0 kudos

Not able to read AES256 encrypted data from microcontroller using UART. I am used the STM32L442KC microcontroller. I am new for AES Encryption / Descryption.

I am using atolic truestudio 9.3 . myplaintext is a[1]={97}; uint8_t ciphertext [32]; my code is below, uint32_t retval=HAL_CRYP_AESECB_Encrypt(&hcryp, plaintext, 8, ciphertext, 5);  if(retval==0)  {  HAL_UART_Transmit(&huart1,(uint8_t *)...

STAR by Associate II
  • 776 Views
  • 0 replies
  • 0 kudos

Getting AES_ERR_BAD_OPERATION on SE_Decrypt_Append

Hi,I'm in the process of implementing a HTTP server in SBSFU where I can upload an update file from a webpage. I've based my work on the code in sfu_loader.c, specifically the function SFU_COM_YMODEM_DataPktRxCpltCallback() and I try to follow the sa...

Arno1 by Senior
  • 971 Views
  • 1 replies
  • 0 kudos

Does X-CUBE-SBSFU support the external flash on the SPI ?

Does X-CUBE-SBSFU support the external flash on the SPI for the secure boot and secure firmware updates ? If yes could you please provide more details if there is any reference boards which has this support. Thanks in Advance,Best Regards,Gowda

MGowd.11 by Associate II
  • 2162 Views
  • 5 replies
  • 0 kudos