Does X-CUBE-SBSFU support the external flash on the SPI for the secure boot and secure firmware updates ? If yes could you please provide more details if there is any reference boards which has this support. Thanks in Advance,Best Regards,Gowda
Hello Jocelyn,Thanks for the reply, by mistake I missed to use "reply" while writing to you, I am writing my question again. Is there any example reference with the normal SPI mode supporting the external flash on STM32L496 in SBSFU 2.3.0?If not, is ...
Hello Jocelyn,Thanks for the reply.Is there any example reference with the normal SPI mode supporting the external flash on STM32L496 in SBSFU 2.3.0?If not, is it straightforward to integrate the existing external flash memory drivers on STM32L496 a...