STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to remove sbsfu code

Hi support team,i am testing the sbsfu code in P-NUCLEO-WB55 but i missed out to disable security ips SECBOOT_DISABLE_SECURITY_IPS and flash into the board it set RDP level to 1 also set SFU_WRP_PROTECT_ENABLE, SFU_TAMPER_PROTECT_ENABLE,SFU_DAP_PROTE...

asala.19 by Associate III
  • 2456 Views
  • 5 replies
  • 0 kudos

Resolved! SBSFU : how to remove write protection?

Hi,I forgot to comment the protections set in app_sfu.h and tried debugging the code. Later I realized and commented everything and it is not allowing me to flash the program on the device. I made RDP level 0 from cube programmer, but still write pro...

ANaga.2 by Associate II
  • 7760 Views
  • 5 replies
  • 0 kudos

Crypto library RSA Signature errors

Hi,I am trying to use the STM32Cryptography library to verify the signature of a flash segment, using RSA Encryption and 3072 bit length keys.The signature is generated by a python script and appended to the hex file. The signature has a length of 38...

On the STM32H (not L) I need to use a 1-wire EPROM, and I try the generic driver calls generated by the IDE (HAL_SWPMI_Receive, HAL_SWPMI_Transmit, HAL_SWPMI_MspInit, etc.) and I see no bits going out on the scope, and the transmit times out.

I can "Transmit" but the TXE flag never clears and the transmit times out. It's unclear which parts of the bus are fully automated (reset, discovery, etc.) and how much of the CRC is handled, etc. I can see nothing on a scope, but if the chip gets in...

PBrai.1 by Associate
  • 2216 Views
  • 2 replies
  • 0 kudos

Resolved! STM32H735RGV6 and STM32H725RGV6 software compatibility?

We have a design based on STM32H735RGV6. We are trying to move our design to STM32H725RGV6.These two MCUs are pin compatible and can be used in the same design without changing the board design.However, we are not sure about using the same software i...

STM32H753 - generating SBSFU bin file

We are facing an issue related to the STM32H753 MCU , CubeIDE version 1.10.1 .We compiled our project successfully with all needed scripts for generate the SBSFU file + sfb bin file.The bin file programmed into the internal FLASH via the Cube Program...

AHada.2 by Associate
  • 1739 Views
  • 1 replies
  • 0 kudos