STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Implement Key replacement package for Image signing Key ECCKEY1

The SBSFU framework allows users to employ multiple image signing keys, ECCKEY1, ECCKEY2, and ECCKEY3.Is there a method to blacklist ECCKEY1 and replace it with ECCKEY4, which may be transmitted via a key replacement update package if the private key...

Grogu by Associate III
  • 1181 Views
  • 2 replies
  • 0 kudos

Big packed BIN image if some code execute in ITCM.

I complie STM32F769I-Discovery 2_Images. the final SBSFU_UserApp image's size is 532kb, It's size will increase to 131,669 kb if ITCM used. I add below code to UserApp.sct ;ITCM 16k ITCMRAM_region 0x00000200 0x00004000 { fw_update_app.o (+RO...

tercelcn by Associate II
  • 2343 Views
  • 4 replies
  • 0 kudos

SECoreBin postbuild script incorrectly updates PATH

I'm using SBSFU v2.6.2 on a Windows 10 x64 machine with CubeIDE v1.11.0I was recently modifying the postbuild script in an SBSFU-based project and noticed it has a bug setting the PATH variable when looking for prepareimage executable:export PATH=$ba...

How to remove sbsfu code

Hi support team,i am testing the sbsfu code in P-NUCLEO-WB55 but i missed out to disable security ips SECBOOT_DISABLE_SECURITY_IPS and flash into the board it set RDP level to 1 also set SFU_WRP_PROTECT_ENABLE, SFU_TAMPER_PROTECT_ENABLE,SFU_DAP_PROTE...

asala.19 by Associate III
  • 2411 Views
  • 5 replies
  • 0 kudos

Resolved! SBSFU : how to remove write protection?

Hi,I forgot to comment the protections set in app_sfu.h and tried debugging the code. Later I realized and commented everything and it is not allowing me to flash the program on the device. I made RDP level 0 from cube programmer, but still write pro...

ANaga.2 by Associate II
  • 7667 Views
  • 5 replies
  • 0 kudos