STM32 MCUs Security

Ask questions and find answers on STM32 security frameworks and tools, including cryptographic libraries, TrustZone, and the Secure Manager.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SIL Rating

I have a question regarding the use of STM32F4 devices in IEC 61508 SIL2/SIL3 applications. The STM32 Safety Library documentation indicates that STM32 devices can be used in SIL2/SIL3 applications. However, I could not find an explicit Hardware Syst...

Him_ by Visitor
  • 32 Views
  • 0 replies
  • 0 kudos

attestation roots for stm32 U3C5

Hi, I have a NUCLEO-U3C5ZI-Q board, and I'm trying to follow the DUA_USER attestation process.   I noticed that the existing Root CA certificates like here https://github.com/STMicroelectronics/STM32CubeU3/blob/main/Utilities/Certificates/ do not ver...

Problems with STM32H5 debug authentication

Test bed:- Nucleo-H503 & Nucleo-H533- Few WeAct H523 connected via Waveshare STLink v2 mini (4 wires only)- my own H503 based controller connected via cheap STLink v2 clones (4 wires only)- I am using STM32_Programmer_CLI v2.21.0 / Ubuntu 24.04 LTSId...

hijax_pl by Associate III
  • 98 Views
  • 1 replies
  • 2 kudos

Most Secure STM32 ?

Hello Team,Good Day !After Cloneed our two version of Hardware ( STM32F3 Series based ) by compititor , we are now more focused on Hardware Security aspects.Can you Pls Suggest which STM32 MCU is the MOST Secure among all available MCU ? Considering ...

bsuthar by Senior
  • 559 Views
  • 10 replies
  • 7 kudos

stm32h573 otp memory

I'm looking for a working example of how to program the OTP memory on the STM32H573.I am looking to program with TrustZone enabled, from secure mode.  I'm using STM32Cube_FW_H5_v1.4.0, and am not in a good position to move to v1.5.0.  Any working exa...

rdl_42 by Associate III
  • 288 Views
  • 3 replies
  • 1 kudos

STM32U585: Start bootloader via RSS command

I have a STM32U585 (edit: ...VIT6, so not the one where this doesn't work due to errata) product with Trustzone enabled, Bootlock disabled and RDP level 0.I want to bring this into ST bootloader mode from software (for easy Firmware change via USB).T...

OliM_1-1778070843232.png OliM_0-1778070786976.png
OliM by Senior II
  • 201 Views
  • 1 replies
  • 0 kudos
Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.