2025-08-16 12:53 PM - edited 2025-08-16 12:54 PM
I'm trying to understand an issue I am having with chaining decryption, using the shared key out of the SAES and have distilled the problem to the following example:
I am attempting to encrypt and decrypt large blocks of data (65536 bytes). I can encrypt and decrypt the entire block in one fell swoop with one call to Encrypt and one call to Decrypt. I can encrypt and decrypt the entire block in small chunks with repeated calls to Encrypt and Decrypt back to back (En, De, En, De, ...). However if I encrypt the entire block in chunks then decrypt the entire block in chunks (En, En, En, ... De, De De, ...), I get bad data as my decrypted text.
I'm trying to understand what I am setting up incorrectly for the decrypted data to be bad. I'm using a STM32H7S78-DK board, although any STM32H7Sxxx could be used in this example. I am using a clean CRYP_SAES_SharedKey_Appli project. I have added the following code to the project. Any help on this problem would be greatly appreciated:
uint8_t plaintext[65536];
uint8_t crypttext[65536];
uint8_t decryptedtext[65536]; /* Initialise CRYP */
if (HAL_CRYP_Init(&hcryp) != HAL_OK)
{
/* Initialization Error */
Error_Handler();
}
// ADDED
for (int i = 0; i < 65536; i++) {
plaintext[i] = i % 256;
crypttext[i] = 0;
decryptedtext[i] = 0;
}
for (int i = 0; i < 64; i++) {
HAL_CRYP_Encrypt(&hcryp, ((uint32_t*)plaintext) + (128 * i), 128, ((uint32_t*)crypttext) + (128 * i), 0xfff);
HAL_CRYP_Decrypt(&hcryp, ((uint32_t*)crypttext) + (128 * i), 128, ((uint32_t*)decryptedtext) + (128 * i), 0xfff);
}
volatile int cmpret = 0;
cmpret = memcmp(plaintext, decryptedtext, 2048); //<--- THIS WORKS OK
for (int i = 0; i < 65536; i++) {
crypttext[i] = 0;
decryptedtext[i] = 0;
}
for (int i = 0; i < 64; i++) {
HAL_CRYP_Encrypt(&hcryp, ((uint32_t*)plaintext) + (128 * i), 128, ((uint32_t*)crypttext) + (128 * i), 0xfff);
}
for (int i = 0; i < 64; i++) {
HAL_CRYP_Decrypt(&hcryp, ((uint32_t*)crypttext) + (128 * i), 128, ((uint32_t*)decryptedtext) + (128 * i), 0xfff);
}
cmpret = memcmp(plaintext, decryptedtext, 2048); // <--- THIS DOES NOT EQUAL!
HAL_Delay(1);
// END ADD
// /* AES ECB Encryption */
// if (HAL_CRYP_Encrypt(&hcryp, Plaintext, 16, EncryptedText, TIMEOUT_VALUE) != HAL_OK)
// {