Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Viper06LS shuts down over 520 VDC Input Voltage

Hello,I use the Viper06LS in the Buck Converter topology.The input voltage can vary between 100V and 530VDC. The output voltage is regulated to 10 V. (See "Viper_circuit"!)Unfortunately, a problem arises when the input voltage increases to approx. 52...

Scheffel by Associate
  • 1378 Views
  • 0 replies
  • 0 kudos

Resolved! Capacitor at The AUX

Hi, i design a SPMS with VIPER013HS and in the design schematic, i dont know the purpose of the capacitor in attached picture. Also in design, there is no capacitor value mentioned for this capacitor.

capacitor.png

L6235

Hi I want to use a L6235 to control a BLDC motor, but do not have a micro to control the loop.  Micro not an option. The are two options I have is to use an integrator as per datasheet or use app note DT0001 mention using the Tacho output and the FWD...

VNF1048F Reverse current behavior

Hello,I am planning to use the VNF1048F as a eFuse for my current project.From the datasheet it is not clear to me which is the behavior of the VNF1048F in case of reverse current.Does it automatically close the MOSFETs (to avoid diode conduction), d...

SPV1050 MPPT resistor

There is confusion about resistor values on input voltage divider.According to datasheet voltage on MPP pin should be lower than 2.1 V (Vuvp - 0.1V)In application note AN4397 you used UVP set by resistors R4, R5, R6? Which value should be used?

es by Associate
  • 858 Views
  • 0 replies
  • 0 kudos

Recherche transistor

Bonjour,Je viens d'ouvrir un ventilateur de refroidissement sur audiIl y a 7 transistors dont 2 sont cramé Il y a écrit dessus ST604342Mais impossible de trouver quoi que ce soit sur la toile.Quelqu'un peut-il m'aider Merci d'avance 

Cu2w by Associate
  • 2101 Views
  • 2 replies
  • 0 kudos

Resolved! STP24DP05 IC queries

Hi Team, We are using this STP24DP05 (24-bit constant current LED sink driver with output error detection) IC for a X*Y array of diodes to get high or low. The IC is interfaced with microcontroller using SDI pin of STP24DP05. We have some doubts kind...

Meghla by Associate II
  • 4143 Views
  • 9 replies
  • 0 kudos