Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Issue with PWD13F60 driving dc brushed motor

I am using a EVALPWD13F60 and a stm32f103c8 bluepill to drive a small DC brushed motor. When duty cycle is above about 30%, the motor starts to oscillate. I couldn't figure what's wrong with my circuit and code. thanks.

0693W00000Y6yEBQAZ.jpg
DZhou.4 by Associate
  • 227 Views
  • 1 replies
  • 0 kudos

Reading from STPM32 ic by STM32F103. is it an Error?

Hi Guys,I use STM32F103 with STPM32(single phase electric meter ic) evaluation board. i used of stpm002 firmware to connect with stpm32 and read measured data from it. like RMS voltage and.....  I want activate LED1(It connected to pin 4 of STPM32) ,...

0693W00000QO64RQAT.jpg

How to control stusb1602 using stm32f103

I wanna to implement USBPD with stusb1602 and stm32f103.have 3 USBPD Port and implement control and operation with stm32f103.but i could not find any related information. According to document, that need to use stm32f072 to implement USBPD. ans so is...

MLee.14 by Associate
  • 421 Views
  • 3 replies
  • 0 kudos

community.st.com

Posted on May 08, 2017 at 17:03Why does my BLDC motor stop during acceleration 2 ? Hello,I bought a STSPIN32F0 and i try to run this board with a BLDC Motor. But the first 3-4 seconds is working then stops. The same problem with me onhttps://communi...