Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! STP24DP05 IC queries

Hi Team, We are using this STP24DP05 (24-bit constant current LED sink driver with output error detection) IC for a X*Y array of diodes to get high or low. The IC is interfaced with microcontroller using SDI pin of STP24DP05. We have some doubts kind...

Meghla by Associate II
  • 4164 Views
  • 9 replies
  • 0 kudos

VNF9Q20F OUT CONTROL USING DIO PINS

Hi Everyone,    I'm working on VNF9Q20F and VNF9D5F , I have an issue where I can’t control OUT (ON/OFF) BY SPI or by DIO .    Once the VNF is in normal mode. Below are the commands which are I ‘m sending: 0x0h: 0x0 0x00 0x3F 0xF1,0x03h: 0x0 0x03 0x3...

STC3115 wrong SOC estimation

Good morning,I'm currently using the STC3115 in my application for estimating the SOC of a 1000mAh LiPo battery.The application drain a quite costant current, between 20 and 25mA, so the coulomb counter should be an easy approach for monitoring the S...

matteoriga_0-1724756296759.png

STC3100 Calibration

Hi together, ive read in the Datasheet that the STC3100 can be calibrated.The GG_CAL Bit (Bit 3 in REG_MODE @ Adress 0) can be set to short the analog Inputs together, allowing to compensate for Offset Errors.But how do i have to use this Bit? Just s...

SPV1040 Light Load Efficiency

What is the SPV1040 MPPT Charger's light load efficiency? In my application, the power from the Solar Panel goes down to 10mW. So, I'm interested, to know the output of SPV1040T when the input power is only several mW.  From the datasheet, my applica...

Stalin_0-1725703826682.png
Stalin by Associate III
  • 1441 Views
  • 2 replies
  • 0 kudos

Resolved! SPV1050 No Voltage at the LDO-Out Pins

Hi all,I connected my SPV1050 chip as you can see in the picture and started to measure my circuit. It looks pretty good. I powered it up with 3.3V at IN_LV. And I can measure a voltage of about 2.416V at the STORE pin. And even the LDO2_EN pin got a...

SPV1050.png

About VNL5030JTR-E,VNL5050S5TR-E,VNLD5160TR-E

Thank you for your help.What V/μs is the maximum allowable value of dV/dt for the following components?Please let me know. VNL5030JTR-EVNL5050S5TR-EVNLD5160TR-E Thank you for your cooperation. Yukio IchikataiNIKKI CO.,LTD.

Ichi by Associate
  • 649 Views
  • 0 replies
  • 0 kudos

Resolved! Need of ROHS compliance document

We need ROHS compliance documents for (STM811SW16F, ESDA25W5, TSC214ICT) these part numbers, can you please share the document for further use.

Brindha by Associate
  • 1929 Views
  • 2 replies
  • 0 kudos

STNS01 not shutting down properly

Hello, I have a simple circuit with an STNS01 charging a 150mAh single cell battery and am using the LDO to power an STM32F042 and a couple of other small devices. It mostly seems to work OK, however if I pull the SD line high using the micro (or an ...

miket6000 by Associate II
  • 2884 Views
  • 2 replies
  • 0 kudos