Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! Need help setting up STEVAL-3DP001V1

Hello,I got this board and connected power and could not see any activity on the ST-LINK USB port (J11). I installed the drivers and used 115200,8,N,1, no flow control. There's no startup message or response to CR or serial echo.I can connect to the ...

Jim1 by Associate II
  • 925 Views
  • 6 replies
  • 1 kudos

SW4ST build of X-CUBE-SPN7 demo project

Posted on June 11, 2017 at 20:47♯ build using ♯&sharpen.X-CUBE-SPN7.zip  Running an up-to-date Eclipse Ac6 session here is what happens when I try to build the &sharpX-CUBE-SPN7 demo application:1.select  File menu item2.   select Open Projects from...