Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

GUI L99615C Software issue

Hello,I have a problem with connection L99615 with dedicated software STSW-L99615C. First of all, there is no automatic connection to the com port (I read that it is possible, so I made it manually but it still looks strange - one time I saw that my ...

jojoanaa by Associate
  • 259 Views
  • 0 replies
  • 0 kudos

STEVAL-SPIN3201 disk size.

When I connect the board, the SPIN32F0 removable drive (E:) that Windows sees is only 8KB. Reading User Manual UM2152: "....when the binary size is close to the 32 Kbytes maximum limit of the STSPIN32F0 (this is the case of the example binaries)".Cle...

Liam G by Associate II
  • 598 Views
  • 4 replies
  • 0 kudos

Hello, I am new to STPM34 eval board and trying to getting start to STPM34 eval software. Getting error "unhandled exception error while doing USB interface"

On opening the STPM34 eval software and connecting USB to UART to PC. Under Option>Interface> Communication, I selected Port type as USB and tried to open port.Error window pop up - 'unhandled exception has occurred' as shown in Fig. 2.This error rem...