VN920B5HTR-E Driver's Current Sensor Function Appropriate Resistance Value
Hello, I would like to use the current sensor function of the VN920B5HTR-E driver.According to the data sheet, when the Rsense value is used at 10k, it is expressed as 4V when it is 10A above 8V.I use a load of 12V and up to about 8A, so can I use 10...