Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to get active power with STPM3x..

I am using STPM33.Reading 70 registers using UART was a success.Data received ex)A0 00 E0 04 00 00 00 F8 A0 00 A0 00 E0 04 00 00 00 F8 00 F8 00 F8 00 F8 FF 0F FF 0F FF 0F FF 0F 27 03 27 03 00 00 00 00 7E 77 7E 77 07 40 83 06 00 00 72 10 72 00 08 06 3...

LYoun.11 by Associate
  • 252 Views
  • 0 replies
  • 0 kudos

I am using eval STPM34 for energy meter project. I am connecting ESP32 to STPM34 using UART. i.e. only Tx and Rx are used. I am writing ESP32 code using Arduino IDE. I cannot read any other register data

I am using eval STPM34 for energy meter project. I am connecting ESP32 to STPM34 using UART. i.e. only Tx and Rx are used.I am writing ESP32 code using Arduino IDE.When I use Serial2.read() function to read any register data, I always get "160 0 0 4"...

Max/min application speed cannot read

Posted on June 18, 2018 at 12:35Referring to UM1052, chapter 14.It says that register s 0x3F and 0x40 are available to read using the get register command frame over UART. I have most of the other registers up and running, so the problem is not with...

freppa by Associate II
  • 275 Views
  • 0 replies
  • 0 kudos