Power management

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

STWBC86 stops working after a few days

Hi,I have a array of 2x5 STWBC86 on a aluminium plate to make a charging station for multiple devices. They are all connected to a common 5V source and decoupled by a small filter of Ferrite bead and MLCC.After testing them for a while i let them res...

S3rr4 by Associate II
  • 417 Views
  • 10 replies
  • 0 kudos

Resolved! WBC86TX and WLC38RX inband communication

Hello everyone,I have the STEVAL WBC86TX and RLC38RX evalboard here and I am currently testing them with the STSW-WPStudio.In my application I want to implement an custom inband communication between RX <--> TX. It seems that there is the possibility...

simonh by Associate
  • 506 Views
  • 1 replies
  • 1 kudos

Problems setting up the STWLC38

Hello, We plan to use the STWLC38 for power in a new wearable design. We purchased the STEVAL-WLC38RX and STEVAL-WBC86TX kits to get familiar and experiment with the ICs. Now we are trying to adapt the Rx of the STEVAL-WLC38RX as used in a wearable d...

stwlc38 firmware download issues

We use wireless charger RX IC stwlc38, though we tried to write firmware which provided by the link https://github.com/STwirelesscharger/STWLC38_NUCLEO_L476RG, but we met the CUT id mismatch during firmware writing via I2C interface and then the F/W ...

daveoh by Associate
  • 181 Views
  • 1 replies
  • 0 kudos

STWLC38: GUI connect No response

Hello, I have a custom board with a STWLC38JRM. Everything was fine and I was able to flash it with STSW-WPSTUDIO v1.8.4 through the dev board STEVAL-WLC38RX and FT_SDA/FT_SCL/VBUS/AGND pins. I try to make some test and I disabled internal overtemper...

jbie by Associate II
  • 148 Views
  • 1 replies
  • 0 kudos

FOD on STWBC-MC

 Hello STM community.We developed a wireless charger based on the STWBC-MC chip.Our design follows exactly the ST Eval-Kit STEVAL-ISB047V1.No we are facing a problem with a customer, that the Foreign Object Detection (FOD) does not work stable. In so...

SvenRaecker_1-1710136601114.png

Resolved! STWBC86 GPIO registers

Hello, I'd like to use GPIO00 ... GPIO04 as outputs to select the used coil from a coil array for power transmitting.  I've seen the i2c addresses of the GPIO's configuration at 0x30 and followed. I'm wondering what address is foreseen to read or wri...