Power management

Discuss power management solutions. Ask questions and find answers on voltage configurations, short circuit protection, and programming.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

WLC99Rx Stuck in DC Mode

I'm getting a STEVAL-WLC99RX and STEVAL-WBCTX70 configured for some testing and put the WLC99RX in DC mode (5V ono Vout). I cannot figure out how to get it back into Rx mode.It feels a little bit like a chicken and egg situation. I need to be in DC m...

Electrically Isolated Semiconductor Device - STGF15H60DF

I had previously asked in case # 00204067, if the subject part STGF15H60DF was UL approved for isolation and I was told that is was approved under UL catigory QQQX2.E81734 per the requirements of UL 1557. I was linked to UL File # E81734 with a highl...

Dart-Eng by Associate
  • 2052 Views
  • 2 replies
  • 0 kudos

GP244

Hi,This is a over voltage diode from a uC programmer that I blew. Can anyone tell me the value? Thank you for the help,Rob

Robaroni by Associate
  • 940 Views
  • 1 replies
  • 0 kudos

L6235Q - Using DIR with PWM signal (DT0001)

I found an aplication (ST Design Tip - DT0001), that suggests a way of controlling motor speed, using a PWM signal on the DIR input.  Works fine for speed.  Note: we are not using a micro as shown in the DT90001. We are using our design.  And using P...

MikeSD by Associate
  • 1335 Views
  • 1 replies
  • 0 kudos

Resolved! L6902 component choice

Hi, I'm designing a DIY switching power supply around the L6902. Intended output voltage is <22V, input voltage 24V, output current in constant current mode between 0.6 and 0.8A.My questions:the datasheet shows an inductor value of 22uH, is this valu...

Tfive by Associate II
  • 15971 Views
  • 16 replies
  • 1 kudos

Resolved! Using MPP on stwlc38

Is it possible to use a Qi2 rx coil with magnetic array on a stwlc38 design? The goal is to use a Qi2 charger and reap the benefits of magnetic alignment and 15W charging while still being on the Qi1.3 standard of the stwlc38.

Jvan .23 by Associate II
  • 2849 Views
  • 4 replies
  • 0 kudos