User Activity

Hi All,I have developed my own Evalboard for the STWBC2-HP based on the STEVAL-WBC2TX50. Now i have flashed the stdes-50w2cwbc_FW_v1.0.0.0.hex firmware to the board and the Software shows the following. The power transfer does not work. Do you have a...
Hello,I have developed my own evaluation Board for the STWLC98 Chip. When connecting the power suplly, the DC-Mode, which is on the IC when it is delivered, works in a correct way. But when I want to program the IC with the following firmware from th...
Hello,Is there already a solution available to use the STWLC98 or the STWLC38 in TX mode? Is there any application note or some other more detailed description for the TX mode? My problem is the following:I want to transmit 15W, but the STWBC86 can o...
Hello everyone,I have the STEVAL WBC86TX and RLC38RX evalboard here and I am currently testing them with the STSW-WPStudio.In my application I want to implement an custom inband communication between RX <--> TX. It seems that there is the possibility...
Kudos from
Kudos given to