Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Resolved! How do I select different output voltages from the STUSB4500 without using a microcontroller?

I want to use a STUSB4500LBJR for USB-C power delivery. On the datasheet stands that connecting the I2C lines is optional and in another datasheed of the STUSB4500 stands that I don't have to use a microcontroller. But I cannot find information about...

Reading from L9663 PSI5 Transceiver

Hello,I am using L9663 PSI5 transceiver for the development of a steering drive project. I have a doubt regarding the SPI communication. If I want to read a register content will I be able to get it in the same MISO data?For example, I am sending a 3...

VRaja.3 by Associate
  • 1006 Views
  • 1 replies
  • 0 kudos

L9663 SYNC pulse trigger via SPI

Hi!Can somebody help, what is the SPI command for triggering sync pulse on PSI5 channel? Auto generated sync pulse mode works fine but i can not find the corresponding SPI command for sync pulse triggering in datasheet.I would like to use the followi...

Livius by Associate II
  • 1115 Views
  • 1 replies
  • 0 kudos

My STEVAL-IDB011V1 board Unable to download firmware

When i use WISE Studio Build the demo project, Then Run;There comes the problem.My computer can recognize the board.Also The BlueNRG GUI Tools can read DK Serial port .But can not Successfully connected.​​There also the BlueNRG-LP Navigator tools.I d...

0693W00000QOMYMQA5.png 0693W00000QOMZ0QAP.png 0693W00000QOMa8QAH.png 0693W00000QOMarQAH.png
elv.1 by Associate II
  • 1605 Views
  • 2 replies
  • 0 kudos

Which BOM to use for SMPS for BlueNRG-LP: the one from Reference Manual (RM0479 Rev1) or from STEVAL-IDB011V2 - Rev 1 ?

Hi everyone,I'm confused in regars of BOM for SMPS for BlueNRG-LP. In the Reference Manual we can see the following recommandation: and in the document for the evaluation board there is another solution:  Would it be possible to get an answer if both...

0693W00000StxJnQAJ.jpg 0693W00000StxKHQAZ.jpg
GBedn.1 by Associate II
  • 1729 Views
  • 2 replies
  • 0 kudos