Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Should Pin 21 of BLUENRG-M2SA be grounded?

Hello,I am using the BLUENRG-M2SA in my design. In the BLUENRG-M2 datasheet at https://www.st.com/resource/en/datasheet/bluenrg-m2.pdf, it is stated that all GND pins must be grounded. However, in the BLE module integration design guidelines (DT0142)...

ASang.2 by Associate
  • 1892 Views
  • 4 replies
  • 0 kudos

STEVAL-IDB008V1M ADC Input 1 & 2 connections

Hello, I've been using the STEVAL-IDB008V1M to help develop an BLUENRG-M2 product for an company. I've noticed in the schematic there are 3pF capacitors connected to the ADC Input 1 and Input 2Does anyone know why this is done?For the time being I ha...

0693W00000BcjVdQAJ.png
BWill.4 by Associate
  • 1588 Views
  • 1 replies
  • 0 kudos

BlueNRG-M2 Host-less mode

Dear all, I'm just getting started using a BlueNRG-M2 module and a host STM32.Browsing through the documentation I've seen that chapter 3.2 of bluenrg-m2 datasheet mentions "Host-less mode (application processor): customer application runs on the Blu...

app_processorVsnetwork_processor.png

S2_LP SMPS inductor

Hi,We want to use the S2-LP with embedded SMPS enabled. The recommended inductor value is 10uH.We need to lower the inductor value. I have read  that it would be possible to reduce the inductor value to 2.2uF in  the AN5246How to use SMPS to improve ...

Adalgiso by Associate II
  • 1560 Views
  • 1 replies
  • 0 kudos