cancel
Showing results for 
Search instead for 
Did you mean: 

"absolute maximum" rating vs "operating" conditions

NMP.1
Associate

E-TEA3718SFPTR is used for stepper driving

actually the package is S020.

In datasheet absolute maximum rating is mentioned as 45V for Vs.

But in operating condition, it is mentioned 10v for S020 package.

Please clarify?

This discussion is locked. Please start a new topic to ask your question.
1 REPLY 1
Peter BENSCH
ST Employee

Welcome, @NMP.1​, to the community!

Some information in the heading of Table 5 unfortunately contains some typos. The datasheet rev 2 says:

  • Symbol | Parameters | SO20 | Power DIP | Multiwatt 15 | Unit

but it should read as:

  • Symbol | Parameters | Min. | Typ. | Max. | Unit

Sorry for the confusion!

Does it answer your question?

Regards

/Peter

In order to give better visibility on the answered topics, please click on Accept as Solution on the reply which solved your issue or answered your question.