Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

Activate bootloader on BlueNRG-2N

Hi,I'm having problems to activate the built-in BlueNRG-2N bootloader. I put DIO7 high (Boot) and perform a reset (/Reset 5ms low then high again).Then I wait 150ms to give the bootloader a little time to initialize. Then I send 0x7F on the UART-line...

H W by Associate II
  • 1188 Views
  • 1 replies
  • 0 kudos

BlueNRG-2N bootloader "Get ID" command

Hi,I'm asking the bootloader of an BlueNRG-2N for the "Get ID" command and it responds 0x02 0x01 0x4F.The upper nibble of the last byte ist 4. But 4 is not mentioned in AN4872.4 means ???2 means BlueNRG-20 means BlueNRG-1Any hints?Regards.

H W by Associate II
  • 762 Views
  • 0 replies
  • 0 kudos

BlueNRG2 BLE timeout

I am using the BlueNRG2 in an application which is a simple button press to indicate if it is pressed or not. The device needs to connect to Windows 10 and or 11. I am using the SensorDemo project as the base code and made a few changes to just utili...

JWall.1 by Associate II
  • 1862 Views
  • 1 replies
  • 0 kudos

Choosing a Bluetooth Module and Dev Tools

We are looking to add a pre qualified bluetooth module to a consumer product and the device live outdoors and periodically connect to a phone. We have identified the BlueNRG-1 as a candidate but perhaps there is a better choice. How well is the BlueN...

PNada.3 by Associate II
  • 896 Views
  • 0 replies
  • 0 kudos