Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

BLE Whitelisting

My BLE (BlueNRG-MS) application has to offer the following functions and I'm not sure what's the correct approachI need to have a pairing mode where a central device can connect. I think this is achieved by using aci_gap_set_discoverable() with NO_WH...

aj.sk by Associate III
  • 6691 Views
  • 7 replies
  • 0 kudos

Not able to send data from BlueNRG LPS

Hi Everyone,I'm using BlueNRG LPS as a network co-processor with STM32L4 Nucleo Board. I'm sending 30 bytes data in every 10ms from stm32 to bluenrg LPS in Non-Block manner, and after 3000 bytes I have to send to packet end command (blocked). So ther...

rshar.21 by Associate II
  • 876 Views
  • 0 replies
  • 0 kudos

TX problem with S2-LP

Hello.I have a problem with S2-LP. I can’t switch S2-LP on a custom board to the TX state. I get the error 0x14 "Error state due to a failure in LOCK operation". The same firmware with the module RC-S2LP-868 works without errors. As an example for th...

ST2378E is not working properly. TT

Hi. I have two level shifters, ST2378e and ADG3308.But, all of them are not working propoerly. Oscilloscope displayed following video.https://youtu.be/JwTMTi1wS8w I had connected pins properly and checked many times.VL(3.3v), VCC(5.0v) and GND OE pin...

Sellyette by Associate II
  • 1131 Views
  • 1 replies
  • 0 kudos