EVKITST87M01-1 development kit
Hi,There is an introduction on the EVKITST87M01 development kit in the flyer found here: fl2311st87m01.pdf, however, I could not find anywhere online to purchase it. Just wondering if it is available yet?Thanks,Olive
Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.
Hi,There is an introduction on the EVKITST87M01 development kit in the flyer found here: fl2311st87m01.pdf, however, I could not find anywhere online to purchase it. Just wondering if it is available yet?Thanks,Olive
Hi,Is it possible to get the used BLE data channel of the last connection interval?I would like to more or less create a bar chart containing the 37 data channels and rssi values of the GATT connection for quality comparisons. Reading the rssi value ...
Hi, I'm just starting out with embedded programming & electronics so please bear with me :)I am starting a project based on the STM32F103 Nucleo board. The first thing I want to do is create a USB host port to connect a class-compliant MIDI device.Fr...
I'm using the BlueNRG-M2 as my processor on an enclosed system with UART communication. My goal is to add the ability to update the firmware via this connection using the built-in bootloader.Using this answer, I am able to activate the bootloader wit...
Hello,In different project with S2-LP we want to read raw the for understand and anlyze any data of the communicate between 2 devices.Are we take tke raw data?Is the S2-LP support E527 standart?Thanks Melih
HiAs i can see your eSIMs come with Truphone preinstalled, so i wonder if its possible to use differrent provider.And if it is, how can you do so on examle of B-L462CELL1
Error observed: From dmesg: tpm tpm0: tpm_try_transmit: send(): error -62OS Version:5.15.71TPM Chip: ST33KTPM2XI2CConnectivity: CPU->I2C-> TPM2.0Driver: https://github.com/STMicroelectronics/TCG-TPM-I2C-DRV/tree/5.10.yStep to reproduce the issueExerc...
I did not see this question answered. I did see a related discussion which motivated me to ask: https://community.st.com/s/question/0D53W00001JVdk5SAD/bluenrg-advertise-while-having-a-connectionI was using the BlueNRGLP DK sample application: BLE_...
Hi,I am using the Bluenrg-332ac and the eval board BlueNRG-LPS STEVAL-IDB012V1. I used the 'hci_le_connectionless_iq_report_event' function to extract IQ signals and RSSI. However, the magnitude, which is derived from the IQ samples, fluctuates dram...