Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

How to open an example application project

Posted on April 26, 2017 at 19:45Hi.....i have worked  with 'Getting started with the Contiki OS/6LoWPAN on STM32 Nucleo with SPIRIT1 and sensors expansion boards' and have been successful in creating a 6lowpan network and getting access of the sens...

Resolved! Serial EEPROM Byte and Page Write Endurance

Posted on April 11, 2017 at 11:42Hi There , We are currently working on a project using an EEPROM to store sporadic data. The eeprom is a 24AA512 with 512kbits memory, from Microchip.We use it to store datalogging data from our application. The prob...

eg7963 by Associate III
  • 2536 Views
  • 3 replies
  • 0 kudos

Resolved! Communicating with BlueNRG-MS after waking up the SPI Master (Application Processor)

Posted on April 25, 2017 at 16:22Hi All,I am running BLE peripheral profile application on Mentor Graphics' Nucleus RTOS using STM32 MCU interfaced with BlueNRG-MS module. The application runs successfully and I can connect to the heart rate monitor...

Spirit1 radio

Posted on April 25, 2017 at 05:47I am trying to get MAC layer timestamps to synchronize two Spirit1 radios. Even with using interrupts for timestamping at the transmitter and the receiver, the receiver timestamps show a high variance of about 2 ms. ...

Resolved! AT+S.SETTIME problem

Posted on April 19, 2017 at 21:41I have a SPWF01 with last firmware 3.5 (160129). But i am facing a problem with setup of the time (AT+S.SETTIME).Each time i send the command the module does not answer and make reset after  20 seconds, i send the co...

SPWF01 can't find host IP of AWS IoT server

Posted on February 09, 2017 at 10:32Hello,we are making MQTT client application that should connect to Amazon AWS server. But after my application sends:AT+S.SOCKON=XXXXXXXXXXXXXX.iot.eu-west-1.amazonaws.com,8883,s,ind<CR>I got an error:ERROR: Faile...

N S by Associate II
  • 5412 Views
  • 14 replies
  • 0 kudos