Interface and connectivity ICs

Ask questions and find answers on connectivity ICs, focusing on protocols and I2C challenges on STM32 Nucleo boards and BlueNRG products.

cancel
Showing results for 
Search instead for 
Did you mean: 

Forum Posts

SPIRIT1 on permanent LOCKWON status

Posted on March 14, 2017 at 14:21Hello,I'm a newbie to the RF world. I'm trying to connect an SPIRIT1 to an Arduino. So far, i was able to communicate with the spirit1 through the SPI interface. However when i send a LOCK or RX/TX command to the spi...

Resolved! User guide for creating Filesystem Images (SPWF04Sx)

Posted on June 26, 2017 at 14:52HiIs there any form of user guide/README.txt for how to create filesystem images using STMicroelectronics\OTA-Images\FS\utils\bin\Windows\CreateFS  (dir2img.bat)I've previously used httpd_gen.exe and gen.bat for files...

Marc ZK by Associate II
  • 1402 Views
  • 3 replies
  • 0 kudos

Multiple race conditions and bugs in SOCKD

Posted on November 20, 2016 at 18:43The SOCKD implementation suffers from many race conditions and bugs which makes it impossible to make robust applications without forcibly rebooting the WiFi module when it's not performing as expected.Problems & ...

mafredri by Associate II
  • 2792 Views
  • 8 replies
  • 0 kudos

BlueNRG stops advertising after some time

Posted on September 28, 2015 at 19:19Hi, I'm having trouble with advertising: it seems that after some time, the module stops advertising. The actual time after the issue appears seems to be grossly related to the Advertising_Interval_Min & Advertis...

hardware by Associate II
  • 4104 Views
  • 13 replies
  • 0 kudos

BlueNRG1 as SPI slave

Posted on June 21, 2017 at 11:55hi,i would like to know if there is any software for STEVAL-IDB007v1  BlueNRG1 as peripherial using SPI bus, tried DTM_SPI.hex but SPI seems not responsive.

oriol by Associate
  • 637 Views
  • 0 replies
  • 0 kudos

Yet another SPI SPWF04S problem

Posted on June 14, 2017 at 12:07 Hi all. I'm having trouble connecting to AP with SPI mode. I tried to same network with putty and USB-to-UART cable and it connected fine (I only did ping over the connection, so not much). However with SPI it con...

Announcement

We’re moving the ST Community to a new platform to give you a better and more reliable community experience.